Copy Work Location Non-Drawn CUs

If you have added non-drawn CUs to a Work Location, you can copy and paste them into another Work Location. To do so, follow these steps:

  1. After adding non-drawn CUs to a Work Location, in the Project pane hover over the Work Location that has the non-drawn CUs. The Options icon appears.

  2. Hover over the Options icon, then click the Copy WL Non-Drawn CUs tool.

  3. Move your cursor to the next Work Location, hover over the Options icon, then click the Paste WL Non-Drawn CUs tool.

As seen in the following animation, you can click paste multiple times. The application increments up the number of non-drawn CUs with each click.

TIP: You can both copy and paste non-drawn CUs using the Click Wheel on Work Locations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?