Pan and Zoom to CUs

With large designs, it can be easy to get lost in the mix, geographically speaking. Luckily, in the Project pane you can quickly choose a CU and navigate to its location.
IMPORTANT: Navigation is available for drawn CUs. While you cannot navigate to a Non-Drawn CU (it does not have a geography itself), you can still navigate to its parent, Driving CU.
  1. In the Project pane, find the CU.
  2. Hover over the options icon for that item, then click the Pan and Zoom to tool.

    TIP: Any time you select a CU in the Project pane, it selects in the map. And, any time you select a CU in the map, it selects in the Project pane.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?