Facility ID

The Facility ID displays at the top of the Component Information pane.

Typically, the application communicates with a service to automatically generate the Facility IDs.

You can also change the Facility IDs. For features you placed in your design, double-click the Facility ID (the text adjacent to the pencil icon) to type a new Facility ID.

IMPORTANT: If you have a process that retrieves Facility IDs from another system, that process does NOT override your manually populated Facility ID.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?