Conductor

A conductor is a linear feature with single or multiple phases.

Sketching

  • Click in the map to place a new conductor. Each click adds a vertex, and a double-click finishes the sketch.

  • Conductors snap to other conductors and devices and inherit phasing. If sketching a single-phase conductor onto a multiple-phase conductor, you are prompted to choose the appropriate phase once sketched.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?