Project Pane

The Project pane is an integral part of Designer XI . It contains several helpful tools to manage the CUs in your design, and it acts as a home base for your inventory while you are working.

IMPORTANT: When you first open the Project pane, there is a default Work Location called “No WL.” This is where newly-placed CUs appear initially. Once you create additional Work Locations, you can drag and drop the CUs into the desired Work Location or use the Auto Assign Work Locations tool.

In the Project pane, you can:

  • Change CUs

  • Add Non-Drawn CUs

  • Change CU quantities or lengths

  • Navigate to CUs or Work Locations

  • Collapse all listed items for easier navigation

  • Delete CUs or Work Locations

  • Manage Work Locations

  • Copy inventory lists by Work Location

  • Update Facility IDs

Keep reading the topics below to learn specifics about the Project pane functions. Topics are organized alphabetically by tool or function name.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?