Gas Utilities

The topics in this help chapter apply to gas utilities, or in the case of utility-neutral functions, use gas assets as their example.

IMPORTANT: A basemap is required for the application to be able to open a design. If you are connected to the internet, then it can stream a basemap. However, if you are planning on doing work while disconnected from the internet, then you must download a package prior to going offline. Go to My Work > Settings to download a package that includes a basemap.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?