Map Clipper

Use the Map Clipper on the Print tab to crop the map on the page.

To use this tool, follow these steps:

  1. On the Print tab, orient your design on the page as needed.

  2. Click the Map Clipper tool.

  3. Bring your cursor into the map.

  4. Click to sketch the extent of the clip box. Each click places a vertex (or bend) in the clip shape.

  5. Double-click or press Enter to finish.

  6. Notice only the area within your clip box is visible.

  7. Optionally, click the Clear Map Clipper tool to return the map to its full size.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?