Maps Pane
The Maps pane provides the ability to change the look and feel of the map features, toggle reference layers, change the underlying basemap, and work with CAD data. More information about all these functions is provided in subsequent help topics.
The pane has four areas:
-
Design
-
Reference
-
Backdrop
-
CAD
Under Reference are four tools:
-
Inspect
-
Add Data
-
Add Reference Design
-
Refresh Layers

Under CAD there are five tools:
-
Import CAD File
-
Adjust CAD
-
Export Design to CAD
-
Move CAD File to Current Extent
-
Zoom to CAD File