Notifications

The Notifications pane is where most of the messaging from the application occurs, including informational messages, warnings, and errors

To open the pane, click the icon in the upper, right-hand corner of the application. The number displayed changes to indicate the number of notifications awaiting action

IMPORTANT: If there are no notifications to read, you will see a gray flag icon. You can still click the flag icon to open the Notification pane.

When you click the icon, the Notifications window opens to give you more information.

When you do have an error in your notifications, the application tells you what the error is and attempts to provide next steps for you to take.

You can dismiss each notification by clicking the Dismiss button on each notification, or you can dismiss them all by clicking the Dismiss All button at the top of the Notifications window.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?