Valve

A valve is a point component.

Sketching

  • Valves snap to pipes.

  • A valve splits an existing pipe into two sections.

  • Once sketched, the device can be operated (open or closed) by phase in the Component Information pane.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?