DOCA0172EN-20

Channel Scan Function

Presentation

Connected IEEE 802.15.4 wireless devices scan other channels to reestablish communication with the Panel Server in the event that communication is lost. If the channel setting for wireless devices is changed manually on the Panel Server webpages, wireless devices scan nearby channels until communication is established. This function can be disabled on compatible devices to help reduce disturbance on other IEEE 802.15.4 wireless devices.

Disabling the scan function is an advanced feature and should be used with caution. You should understand the consequences of the action before disabling it.

Availability

This function is available on Panel Server Entry, Universal (except Wired by Design models), and Advanced.

Setting the Parameters

Dynamic antenna selection is set on the Panel Server webpages, at Settings > Wireless devices > Network configuration.

Managing the Channel Scan Function

To disable the function on the webpages at Manage scan function, click the Scan activation toggle switch. The switch is green when the function is enabled (default configuration) and white when disabled.

NOTE: If not all wireless devices are in connected state, a popup message indicates that the changes have not been saved. Connect all wireless devices and try again.

When the function is disabled:

  • Connected devices do not scan to find a new channel if communication is lost with the Panel Server. They continue to communicate on the current channel at every communication period.

  • It is not possible to modify the channel configuration settings on the webpages. You must reactivate the scan function in order to make modifications to the settings.

Status on wireless device can be one of the following:

  • In progress

  • Applied on all devices

    NOTE: Devices not compatible with disabling of scan function continue to scan.
  • Not applied on all devices

NOTE: If the change is not applied on all devices, check that the firmware version of your devices is compatible with the function. Otherwise click Retry to check that the issue was not a temporary one.

Devices Supporting Disabling of Channel Scan

The following table indicates devices which support disabling of the scan function. The list is not exhaustive.

Device family Device Minimum firmware version

Power meter

PowerTag Rope compliant with IEC and UL standards

001.003.002

PowerTag F160

001.003.002

PowerTag Energy

004.002.000

Ambient sensors

PowerLogic TH110 wireless thermal sensor

001.000.003

PowerLogic CL110 wireless environmental sensor

002.001.003

Wireless CO2 sensor SED-CO2–G-5045

001.001.004

Wireless temperature and humidity sensor SED-TRH-G-5045

001.001.004

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?