Controlled Discovery of Wireless Devices (PowerTag Energy, HeatTag) Through Webpages
Presentation
It is possible to achieve controlled discovery of wireless devices within the Panel Server system. This allows you to apply virtual ID addresses in a defined order, as virtual ID addresses are applied in the order that devices are discovered, and incremented by one for each device discovery.Controlled Discovery Procedure
-
All the wireless devices in the Panel Server system must be powered on.
-
Launch the Panel Server webpage in the web browser.
-
Log in to the webpages (see how to access the webpages).
-
Navigate to
. -
Click Start.
-
Power on the wireless devices, one by one, in the required order.
-
Stop scanning when all the devices are discovered, or click Start again to complete the scanning process.
A list of discovered devices is displayed according to the required order (Modbus address plan).
-
Select the wireless device to configure and click Locate to find the device in the panel.
Result: The status LED of the selected device blinks fast green in the panel.
-
If one of the located wireless devices is not part of your selection, click Delete to reject the device.
-
Once discovery is completed you can view the list of the discovered wireless devices in webpage
. -
Configure the wireless devices.
NOTE: The Modbus address assigned to the wireless devices can be changed after the discovery process is done.