DOCA0265ZH-04

MicroLogic Active 控制单元获取数据

通过手动记录所显示的设置,可以从 MicroLogic Active 控制单元检索设置:

  • MicroLogic Active HMI 上

  • EcoStruxure Power Device 应用

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

这有帮助吗?