Statistic Data
The table lists the statistic data for the PROFIBUS DP communication.
|
Index |
Slot |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|
| 1 | 4 |
0 |
2 |
R |
1 |
ms |
UINT16 |
N |
Timer 1 - Actual value |
| 1 | 4 |
2 |
2 |
R |
1 |
ms |
UINT16 |
N |
Timer 2 - Actual value |
| 1 | 4 |
4 |
2 |
R |
1 |
ms |
UINT16 |
N |
Timer 3 - Actual value |
| 1 | 4 |
6 |
2 |
R |
1 |
ms |
UINT16 |
N |
Timer 4 - Actual value |
| 1 | 4 |
8 |
2 |
R |
1 |
– |
UINT16 |
N |
Counter 1 - Actual value |
| 1 | 4 |
10 |
2 |
R |
1 |
– |
UINT16 |
N |
Counter 2 - Actual value |
| 1 | 4 |
12 |
2 |
R |
1 |
– |
UINT16 |
N |
Counter 3 - Actual value |
| 1 | 4 |
14 |
2 |
R |
1 |
– |
UINT16 |
N |
Counter 4 - Actual value |
| 1 | 4 |
16 |
2 |
R |
1 |
– |
UINT16 |
N |
Thermal overload trip counter |
| 1 | 4 |
18 |
2 |
R |
1 |
– |
UINT16 |
N |
Locked rotor trip counter |
| 1 | 4 |
20 |
2 |
R |
1 |
– |
UINT16 |
N |
Stalled rotor trip counter |
| 1 | 4 |
22 |
2 |
R |
1 |
– |
UINT16 |
N |
Definite time overcurrent trip counter |
| 1 | 4 |
24 |
2 |
R |
1 |
– |
UINT16 |
N |
Normal inverse overcurrent trip counter |
| 1 | 4 |
26 |
2 |
R |
1 |
– |
UINT16 |
N |
Short time overcurrent trip counter |
| 1 | 4 |
28 |
2 |
R |
1 |
– |
UINT16 |
N |
Calculated ground trip counter |
| 1 | 4 |
30 |
2 |
R |
1 |
– |
UINT16 |
N |
Measured ground trip counter |
| 1 | 4 |
32 |
2 |
R |
1 |
– |
UINT16 |
N |
Phase under current trip counter |
| 1 | 4 |
34 |
2 |
R |
1 |
– |
UINT16 |
N |
Current imbalance trip counter |
| 1 | 4 |
36 |
2 |
R |
1 |
– |
UINT16 |
N |
Current phase loss trip counter |
| 1 | 4 |
38 |
2 |
R |
1 |
– |
UINT16 |
N |
Current phase reversal trip counter |
| 1 | 4 |
40 |
2 |
R |
1 |
– |
UINT16 |
N |
Phase under voltage trip counter |
| 1 | 4 |
42 |
2 |
R |
1 |
– |
UINT16 |
N |
Phase over voltage trip counter |
| 1 | 4 |
44 |
2 |
R |
1 |
– |
UINT16 |
N |
Voltage phase loss trip counter |
| 1 | 4 |
46 |
2 |
R |
1 |
– |
UINT16 |
N |
Voltage imbalance trip counter |
| 1 | 4 |
48 |
2 |
R |
1 |
– |
UINT16 |
N |
Voltage phase reversal trip counter |
| 1 | 4 |
50 |
2 |
R |
1 |
– |
UINT16 |
N |
Under frequency trip counter |
| 1 | 4 |
52 |
2 |
R |
1 |
– |
UINT16 |
N |
Over frequency trip counter |
| 1 | 4 |
54 |
2 |
R |
1 |
– |
UINT16 |
N |
Excessive start time trip counter |
| 1 | 4 |
56 |
2 |
R |
1 |
– |
UINT16 |
N |
Communication loss trip counter |
| 1 | 4 |
58 |
2 |
R |
1 |
– |
UINT16 |
N |
LTMT main unit temperature trip counter |
| 1 | 4 |
60 |
2 |
R |
1 |
– |
UINT16 |
N |
Under power trip counter |
| 1 | 4 |
62 |
2 |
R |
1 |
– |
UINT16 |
N |
Over power trip counter |
| 1 | 4 |
64 |
2 |
R |
1 |
– |
UINT16 |
N |
Under power factor trip counter |
| 1 | 4 |
66–78 |
14 |
– |
– |
– |
– |
– |
Reserved |
| 1 | 4 |
80 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 1 trip counter |
| 1 | 4 |
82 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 2 trip counter |
| 1 | 4 |
84 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 3 trip counter |
| 1 | 4 |
86 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 4 trip counter |
| 1 | 4 |
88 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 5 trip counter |
| 1 | 4 |
90 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 6 trip counter |
| 1 | 4 |
92 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 7 trip counter |
| 1 | 4 |
94 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 8 trip counter |
| 1 | 4 |
96 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 9 trip counter |
| 1 | 4 |
98 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 10 trip counter |
| 1 | 4 |
100 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 11 trip counter |
| 1 | 4 |
102 |
2 |
R |
1 |
– |
UINT16 |
N |
DI interlock 12 trip counter |
| 1 | 4 |
104–150 |
8 |
– |
– |
– |
– |
– |
Reserved |
| 1 | 4 |
152 |
2 |
R |
1 |
– |
UINT16 |
N |
Calculator output 1 |
| 1 | 4 |
154 |
2 |
R |
1 |
– |
UINT16 |
N |
Calculator output 2 |
| 1 | 4 |
156 |
2 |
R |
1 |
– |
UINT16 |
N |
Motor stop error detection trip counter |
| 1 | 4 |
158 |
2 |
R |
1 |
– |
UINT16 |
N |
Logic test interrupted trip counter |
| 1 | 4 |
160 |
2 |
R |
1 |
– |
UINT16 |
N |
Stucked reset key trip counter |