Digital Output Settings
The table lists the digital output settings for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 28 |
0 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 1 active type |
| 1 | 28 |
2 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
504 |
Y |
Digital output 1 input source |
| 1 | 28 |
4 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
7 |
Y |
Digital output 1 tag |
| 1 | 28 |
6 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 1 output type |
| 1 | 28 |
8 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 1 pulse time |
| 1 | 28 |
10 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 2 active type |
| 1 | 28 |
12 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
233 |
Y |
Digital output 2 input source |
| 1 | 28 |
14 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
3 |
Y |
Digital output 2 tag |
| 1 | 28 |
16 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 2 output type |
| 1 | 28 |
18 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 2 pulse time |
| 1 | 28 |
20 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 3 active type |
| 1 | 28 |
22 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
234 |
Y |
Digital output 3 input source |
| 1 | 28 |
24 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
2 |
Y |
Digital output 3 tag |
| 1 | 28 |
26 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 3 output type |
| 1 | 28 |
28 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 3 pulse time |
| 1 | 28 |
30 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 4 active type |
| 1 | 28 |
32 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
0 |
Y |
Digital output 4 input source |
| 1 | 28 |
34 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 4 tag |
| 1 | 28 |
36 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 4 output type |
| 1 | 28 |
38 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 4 pulse time |
| 1 | 28 |
40 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 5 active type |
| 1 | 28 |
42 |
2 |
RW |
1 |
– |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 5 input source |
| 1 | 28 |
44 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 5 tag |
| 1 | 28 |
46 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 5 output type |
| 1 | 28 |
48 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 5 pulse time |
| 1 | 28 |
50 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 6 active type |
| 1 | 28 |
52 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
0 |
Y |
Digital output 6 input source |
| 1 | 28 |
54 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 6 tag |
| 1 | 28 |
56 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 6 output type |
| 1 | 28 |
58 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 6 pulse time |
| 1 | 28 |
60 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 7 active type |
| 1 | 28 |
62 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
0 |
Y |
Digital output 7 input source |
| 1 | 28 |
64 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 7 tag |
| 1 | 28 |
66 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 7 output type |
| 1 | 28 |
68 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 1) |
0 |
Y |
Digital output 7 pulse time |
| 1 | 28 |
24 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 8 active type |
| 1 | 28 |
26 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
0 |
Y |
Digital output 8 input source |
| 1 | 28 |
28 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 8 tag |
| 1 | 28 |
30 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 8 output type |
| 1 | 28 |
32 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 8 pulse time |
| 1 | 28 |
34 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 9 active type |
| 1 | 28 |
36 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
0 |
Y |
Digital output 9 input source |
| 1 | 28 |
38 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 9 tag |
| 1 | 28 |
40 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 9 output type |
| 1 | 28 |
42 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 9 pulse time |
| 1 | 28 |
44 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 10 active type |
| 1 | 28 |
46 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
0 |
Y |
Digital output 10 input source |
| 1 | 28 |
48 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 10 tag |
| 1 | 28 |
50 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 10 output type |
| 1 | 28 |
52 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 10 pulse time |
| 1 | 28 |
54 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 11 active type |
| 1 | 28 |
56 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
0 |
Y |
Digital output 11 input source |
| 1 | 28 |
58 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 11 tag |
| 1 | 28 |
60 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 11 output type |
| 1 | 28 |
62 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 11 pulse time |
| 1 | 28 |
64 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 12 active type |
| 1 | 28 |
66 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
0 |
Y |
Digital output 12 input source |
| 1 | 28 |
68 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 12 tag |
| 1 | 28 |
70 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 12 output type |
| 1 | 28 |
72 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 12 pulse time |
| 1 | 28 |
74 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 13 active type |
| 1 | 28 |
76 |
2 |
RW |
1 |
– |
UINT16 |
0–65535 (step 1) |
0 |
Y |
Digital output 13 input source |
| 1 | 28 |
78 |
2 |
RW |
1 |
– |
UINT16 |
0–12 (step 1) |
0 |
Y |
Digital output 13 tag |
| 1 | 28 |
80 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Digital output 13 output type |
| 1 | 28 |
82 |
2 |
RW |
1 |
ms |
UINT16 |
0–60000 (step 10) |
0 |
Y |
Digital output 13 pulse time |
| 1 | 28 |
84 |
8 | – | – | – | – | – | – | – |
Reserved |