Digital Output Status
The table lists the digital output status data for the PROFIBUS DP communication.
| Slot | Index | Byte offset |
Size (in bytes) |
Byte.Bit |
RW |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|
| 1 | 33 | 4 |
1 |
4.0 |
R |
BOOL |
N |
Digital output 1 |
|
4.1 |
R |
BOOL |
N |
Digital output 2 |
||||
|
4.2 |
R |
BOOL |
N |
Digital output 3 |
||||
|
4.3 |
R |
BOOL |
N |
Digital output 4 |
||||
|
4.4 |
R |
BOOL |
N |
Digital output 5 |
||||
|
4.5 |
R |
BOOL |
N |
Digital output 6 |
||||
|
4.6 |
R |
BOOL |
N |
Digital output 7 |
||||
|
4.7 |
R |
BOOL |
N |
Digital output 8 |
||||
| 1 | 33 | 5 |
1 |
5.0 |
R |
BOOL |
N |
Digital output 9 |
|
5.1 |
R |
BOOL |
N |
Digital output 10 |
||||
|
5.2 |
R |
BOOL |
N |
Digital output 11 |
||||
|
5.3 |
R |
BOOL |
N |
Digital output 12 |
||||
|
5.4 |
R |
BOOL |
N |
Digital output 13 |
||||
|
5.5–5.7 |
– |
– |
– |
Reserved |
||||
| 1 | 33 | 6 | 6 |
– |
– |
– |
– |
Reserved |
| 1 | 33 | 7 | 1 | 7.0–7.7 |
– |
– |
– |
Reserved |