Common Trip, Alarm, and Pickup Status
The table lists the common trip, alarm, and pickup status data for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
Byte.Bit |
RW |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|
| 1 | 33 |
28 |
1 |
28.0 |
R |
BOOL |
N |
Pickup status |
|
28.1 |
R |
BOOL |
N |
Alarm status |
||||
|
28.2 |
R |
BOOL |
N |
Trip status |
||||
|
28.3 |
R |
BOOL |
N |
Motor stop error detection |
||||
|
28.4 |
– |
– |
– |
Reserved |
||||
|
28.5 |
R |
BOOL |
N |
Block output |
||||
|
1 |
28.6–28.7 |
R |
BOOL |
N |
Logic test interrupted trip |
|||
| 1 | 33 | 29 |
1 |
29.0–29.7 |
R |
BOOL |
N |
Logic test interrupted pickup |
|
1 |
– |
R |
BOOL |
N |
Stucked reset key trip |