DOCA0256EN-01

Data Addresses

Metering Data

Data Address

Description

5500

L1 RMS current

5502

L2 RMS current

5504

L3 RMS current

5506

Measured ground current

5508

Calculated ground current

5510

Average current

5512

Current imbalance

5513

Current phase sequence

5514

For single phase, L1–N RMS voltage

For three phase, L1–L2 RMS voltage

5516

L2–L3 RMS voltage

5518

L3–L1 RMS voltage

5520

Average voltage

5522

Voltage imbalance

5523

Voltage phase sequence

5524

System frequency

5525

System power factor

5526

Total active power

5528

Total reactive power

5530

Total apparent power

5532

Total active energy

5536

Total reactive energy

5540

Total apparent energy

5544

L1 Current THD

5545

L2 Current THD

5546

L3 Current THD

5547

For single phase, L1–N RMS voltage

For three phase, L1–L2 RMS voltage

5548

L2–L3 Voltage THD

5549

L3–L1 Voltage THD

5550

Temperature measured by PT100 sensor

5551

Temperature measured by binary PTC sensor

5552–5555

Reserved

Motor Data

Data Address

Description

5557

MotorStatus

5558

Thermal Memory

5559

Thermal Time to trip

5561

Thermal Time to cool

5563

Max starts counter

5564

Max start inhibit time

5566

Motor Starting peak current

5568

Motor Starting time

5570

Total run hour

5572

Last run hour

5574

Number of Starts

5575

Number of Stops

5576

Motor Stop Cause

5577

Trip Counter

Last Motor Start Time Stamp

Data Address

Description

5578

Day

5579

Month

5580

Year

5581

Hour

5582

Minute

5583

Second

5584

Reserved

Analog Module Data

Data Address

Description

5585

Analog input 1

5586

Analog input 2

5587

Analog input 3

5588

Analog input 3

5589–5592

Reserved

5593

Analog output 1

5594

Analog output 2

5595–5596

Reserved

Status Data

Data Address

Description

5625

DI Status

5627

DO Status

5629–5637

Reserved

5638

Reserved

5639

Motor Status(Alarm,pickup,trip)

5640

Motor status(stop, start, run, inhibit)

5641

Alarm Bits

5643

Pickup Bits

5645

Trip Bits

5647

Interlock Alarm Bits

5648

Interlock Pickup Bits

5649

Interlock Trip Bits

5650–5655

Reserved

5656

Starter Commands

5658

Motor Run Indicators

5659

Permissive command status

5661

Inhibit Status

5663

ICM - Main Unit

5665

ICM - CTVT

5667

Communication Status

5669

Reserved

Statistic Data

Data Address

Description

5750

Timer 1 - Actual value

5751

Timer 2 - Actual value

5752

Timer 3 - Actual value

5753

Timer 4 - Actual value

5754

Counter 1 - Actual value

5755

Counter 2 - Actual value

5756

Counter 3 - Actual value

5757

Counter 4 - Actual value

5758

Thermal Overload trip Counter

5759

Locked rotor trip counter

5760

Stalled rotor trip counter

5761

Definite time overcurrent trip counter

5762

Normal inverse overcurrent trip counter

5763

Short time overcurrent trip counter

5764

Calculated ground trip Counter

5765

Measured ground trip Counter

5766

Under current trip counter

5767

Current imbalance trip counter

5768

Current phase loss trip counter

5769

Current phase reversal trip counter

5770

Under voltage trip counter

5771

Over voltage trip counter

5772

Voltage phase loss trip counter

5773

Voltage imbalance trip counter

5774

Voltage phase reversal trip counter

5775

Under Frequency trip counter

5776

Over frequency trip counter

5777

Excessive start time trip Counter

5778

Communication loss trip Counter

5779

LTMT main unit temperature trip Counter

5780

Under Power trip Counter

5781

Over Power trip Counter

5782

Under Power factor trip Counter

5783–5789

Reserved

5790

DI Interlock 1 trip Counter

5791

DI Interlock 2 trip Counter

5792

DI Interlock 3 trip Counter

5793

DI Interlock 4 trip Counter

5794

DI Interlock 5 trip Counter

5795

DI Interlock 6 trip Counter

5796

DI Interlock 7 trip Counter

5797

DI Interlock 8 trip Counter

5798

DI Interlock 9 trip Counter

5799

DI Interlock 10 trip Counter

5800

DI Interlock 11 trip Counter

5801

DI Interlock 12 trip Counter

5802–5821

Reserved

5822

Analog Input 1 trip counter

5823

Analog Input 2 trip counter

5824

Analog Input 3 trip counter

5825

Analog Input 4 trip counter

5826

Calculator 1 output

5827

Calculator 2 output

5828

Motor stop error detection trip counter

5829

Logic test interrupted trip counter

5830

Stucked reset key trip counter

Extended Monitoring Data

Data Address

Description

5875

Status word 1

5876

Status word 2

5877

L1 Current (%IFLC)

5878

L2 Current (%IFLC)

5879

L3 Current (%IFLC)

5880

Calculated Ground Trip (%IFLC)

5881

Average Current (%IFLC)

5882

Maximum Current (Imax)

5883

For single phase, L1–N RMS voltage

For three phase, L1–L2 RMS voltage

5884

L2-L3 voltage

5885

L3-L1 voltage

5886

Average Voltage

5887

Total RUN Hour

5888

Last RUN Hour

5889

Motor Starting Time

5890

Motor Starting current(%IFLC)

5891

Active Power

5892

Reactive Power

5893

Apparent power

5894

Active Energy

5896

Reactive Energy

5898

Apparent Energy

5900

Mode status

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?