DOCA0256EN-01

Output Data

Based on the output data size of the data module, the output data can be selected from the following table.

Slot

Index

Byte offset

Size (in bytes)

Byte.Bit

RW Type Svd

Parameter name

1

2

0

1

0.0

RW BOOL N

Motor run forward or High speed forward command

0.1

RW BOOL N

Motor run reverse or High speed reverse command

0.2

RW BOOL N

Local or Remote Mode Sel 1

0.3

RW BOOL N

Trip reset command

0.4

RW BOOL N

Local or Remote Mode Sel 2

0.5

RW BOOL N

Self test (without trip) command

0.6

RW BOOL N

Motor low speed forward command

0.7

RW BOOL N

Motor low speed reverse command

1

2

1

1

1.0

RW BOOL N

Reset Inhibit command

1.1

RW BOOL N

Reset no of starts command

1.2

RW BOOL N

Reset no of stops command

1.3

RW BOOL N

Clear Energy command

1.4

RW BOOL N

Motor Stop command

1.5

RW BOOL N

Logic test command

1.6

RW BOOL N

Reset run hour command

1.7

RW BOOL N

Self test (with trip) command

1

2

2

1

2.0

RW BOOL N

Reserved

2.1

RW BOOL N

Reserved

2.2

RW BOOL N

Clear thermal capacity level command

2.3

RW BOOL N

Reserved

2.4

RW BOOL N

Clear network port settings command

2.5

RW BOOL N

Clear Trip counter command

2.6

RW BOOL N

Reserved

2.7

RW BOOL N

Soft starter reset command

1

2

3

1

3.0

RW BOOL N

Permissive Command 1

3.1

RW BOOL N

Permissive Command 2

3.2

RW BOOL N

Permissive Command 3

3.3

RW BOOL N

Permissive Command 4

3.4

RW BOOL N

Permissive Command 5

3.5

RW BOOL N

Permissive Command 6

3.6

RW BOOL N

Permissive Command 7

3.7

RW BOOL N

Permissive Command 8

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?