LTMT Main Unit with PROFIBUS DP Protocol
Description
The LTMT main unit with PROFIBUS Decentralized-Peripherals (DP) protocol is equipped with two PROFIBUS DP communication ports on the front face.
| A |
Sub-D 9 connector for connection to the PROFIBUS DP network with baud rate up to 12 Mbps |
| B |
Terminal connector for connection to the PROFIBUS DP network with baud rate up to 1.5 Mbps |
Both the ports are functionally identical. They follow the PROFIBUS DP interoperability standards. It is recommended to use the sub-D 9 connector for communication.
Port Settings
The PROFIBUS DP ports have the following configurable settings:
|
Setting |
Setting range |
Default setting |
|---|---|---|
|
Node address |
1–125 in step of 1 |
126 |
|
Product profile |
TeSys Tera |
TeSys Tera |
|
Endianness |
|
Big-endian |
The PROFIBUS DP port settings can be configured using the following interfaces:
-
A PC running the TeSys Tera DTM embedded in a FDT container, such as SoMove software.
-
The LTMTCUF control operator unit.
Node Address
The node address is the address of the LTMT main unit on the PROFIBUS DP bus. You can assign an address from 1 to 125. The factory setting for the address is 126.
You must set the node address before any communication can begin.
Communication Loss Function
Communication loss function detects the loss of communication between the LTMT main unit and the PLC or DCS connected via the communication network, once communication has been established. For more information, refer to Communication Loss section in TeSys Tera Motor Management System User Guide – DOCA0257EN.
Endianness
Endianness is the order in which bytes within a word of digital data are transmitted through a data communication medium. Endianness is represented in two ways:
-
Big Endian:
A big-endian system stores the most significant byte at the smallest memory address and the least significant byte at the largest memory address.
-
Little Endian:
A little-endian system stores the most significant byte at the largest memory address and the least significant byte at the smallest memory address.