DOCA0256EN-01

Overview

Some PROFIBUS DP clients do not provide acyclic service (DP-V1). The PKW feature is implemented to allow acyclic read or write accesses to be encapsulated in cyclic services (DP-V0).

This feature is enabled in the PROFIBUS DP configuration tool by selecting the appropriate module. The PKW data is added to the cyclic data.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?