Output Data
Based on the output data size of the data module, the output data can be selected from the following table.
|
Byte offset |
Size (in bytes) |
Byte.Bit |
RW | Type |
Parameter name |
|---|---|---|---|---|---|
|
0 |
1 |
0.0 |
RW | BOOL |
Motor run forward or High speed forward command |
|
0.1 |
RW | BOOL |
Motor run reverse or High speed reverse command |
||
|
0.2 |
RW | BOOL |
Local or Remote Mode Sel 1 |
||
|
0.3 |
RW | BOOL |
Trip reset command |
||
|
0.4 |
RW | BOOL |
Local or Remote Mode Sel 2 |
||
|
0.5 |
RW | BOOL |
Self test (without trip) command |
||
|
0.6 |
RW | BOOL |
Motor low speed forward command |
||
|
0.7 |
RW | BOOL |
Motor low speed reverse command |
||
|
1 |
1 |
1.0 |
RW | BOOL |
Reset Inhibit command |
|
1.1 |
RW | BOOL |
Reset no of starts command |
||
|
1.2 |
RW | BOOL |
Reset no of stops command |
||
|
1.3 |
RW | BOOL |
Clear Energy command |
||
|
1.4 |
RW | BOOL |
Motor Stop command |
||
|
1.5 |
RW | BOOL |
Logic test command |
||
|
1.6 |
RW | BOOL |
Reset run hour command |
||
|
1.7 |
RW | BOOL |
Self test (with trip) command |
||
|
2 |
1 |
2.0 |
RW | BOOL |
Reset all command |
|
2.1 |
RW | BOOL |
Clear statistics data |
||
|
2.2 |
RW | BOOL |
Clear thermal capacity level command |
||
|
2.3 |
RW | BOOL |
Reset protection settings command |
||
|
2.4 |
RW | BOOL |
Reserved |
||
|
2.5 |
RW | BOOL |
Clear Trip counter command |
||
|
2.6 |
RW | BOOL |
Reserved |
||
|
2.7 |
RW | BOOL |
Soft starter reset command |
||
|
3 |
1 |
3.0 |
RW | BOOL |
Permissive Command 1 |
|
3.1 |
RW | BOOL |
Permissive Command 2 |
||
|
3.2 |
RW | BOOL |
Permissive Command 3 |
||
|
3.3 |
RW | BOOL |
Permissive Command 4 |
||
|
3.4 |
RW | BOOL |
Permissive Command 5 |
||
|
3.5 |
RW | BOOL |
Permissive Command 6 |
||
|
3.6 |
RW | BOOL |
Permissive Command 7 |
||
|
3.7 |
RW | BOOL |
Permissive Command 8 |