DOCA0256EN-01

Interlock Protection Alarm Status

The table lists the interlock protection alarm status data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

Byte.Bit

RW

Type

Svd

Parameter name

1 33

44

1

44.0

R

BOOL

N

Interlock 1 alarm

44.1

R

BOOL

N

Interlock 2 alarm

44.2

R

BOOL

N

Interlock 3 alarm

44.3

R

BOOL

N

Interlock 4 alarm

44.4

R

BOOL

N

Interlock 5 alarm

44.5

R

BOOL

N

Interlock 6 alarm

44.6

R

BOOL

N

Interlock 7 alarm

44.7

R

BOOL

N

Interlock 8 alarm

1 33 45 1

45.0

R

BOOL

N

Interlock 9 alarm

45.1

R

BOOL

N

Interlock 10 alarm

45.2

R

BOOL

N

Interlock 11 alarm

45.3

R

BOOL

N

Interlock 12 alarm

45.4–45.7

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?