Cyclic and Acyclic Services
Overview
In general, the data is exchanged through cyclic service and acyclic services. The application profiles that are supported under cyclic services are:
-
Manufacturer independent data
-
Manufacturer specific data
The fixed set and defined use of manufacturer independent data enables the replacement of a module from the vendor A and by a module from the vendor B.
DP-V0 Services
The DP-V0 services are used for:
-
PROFIBUS DP configuration
-
Cyclic input and output (I/O) data exchange, according to a selected data module
-
Device and communication diagnostics
DP-V1 Read and Write Services
The DP-V1 read and write services enable the access to the acyclic data sets.
PKW Feature
To make this data accessible also for DP-V0 clients, a special feature called Periodically Kept in acyclic Words (PKW), is implemented. In cyclically exchanged data, there are encapsulated request and response frames. They provide access to TeSys Tera systems internal registers.