Motor Start Logs
Description
The LTMT main unit records 250 current values measured during the last motor start.
One log can be saved to serve as motor start reference log.
The last motor start log can be saved as reference log by using:
-
The TeSys Tera DTM.
-
A command from a PLC or DCS via the communication network.
The last motor start log and the reference log:
-
Can be displayed with the TeSys Tera DTM.
-
Are available for PLC or DCS via the communication network.
Two read requests of 256 bytes are necessary to read the last motor start log, and two read requests of 256 bytes are necessary to read the reference log.
Sampling Interval
The sampling interval is based on the trip class selected in the thermal overload settings.
| Trip class | Sampling interval |
|---|---|
| 5 | 20 ms |
| 10 | 40 ms |
| 15 | 60 ms |
| 20 | 80 ms |
| 25 | 100 ms |
| 30 | 120 ms |
| 35 | 140 ms |
| 40 | 160 ms |
Motor Start Log 1
| Slot | Index |
Byte offset |
Size (in bytes) |
X |
Unit |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|
| 1 | 30 |
0 |
8 |
1 |
– |
UINT16 |
Y |
|
| 1 | 30 |
8 |
2 |
1 | ms |
UINT16 |
Y |
Sampling interval |
| 1 | 30 |
10 |
2 |
0.1 | A |
UINT16 |
Y |
IFLC |
| 1 | 30 |
12 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 1 |
| 1 | 30 |
14 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 2 |
| 1 | 30 |
16 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 3 |
|
… |
… |
… |
… |
… |
… |
… |
… |
… |
| 1 | 30 |
238 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 114 |
Motor Start Log 2
| Slot | Index |
Byte offset |
Size (in bytes) |
X |
Unit |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|
| 1 | 31 |
0 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 115 |
| 1 | 31 |
2 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 116 |
| 1 | 31 |
4 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 117 |
| 1 | 31 |
6 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 118 |
|
… |
… |
… |
… |
… |
… |
… |
… |
… |
| 1 | 31 |
238 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 234 |
Motor Start Log 3
| Slot | Index |
Byte offset |
Size (in bytes) |
X |
Unit |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|
| 1 | 32 |
0 |
8 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 235 |
| 1 | 32 |
2 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 236 |
|
… |
… |
… |
… |
… |
… |
… |
… |
… |
| 1 | 32 |
30 |
2 |
0.1 |
%IFLC |
UINT16 |
Y |
Sample 250 |