DOCA0256EN-01

Overview

The PROFIBUS DP is an open industrial standard for integrated communication. It is a serial fieldbus, which provides a decentralized connection between two types of devices:

  • Client devices

  • Server devices

It is a bi-directional network, in which the client device sends a request to a server device, and the server device responds to that request.

The PROFIBUS DP LTMT main unit is a server and supports a PROFIBUS DP application profile based on DP-V0 and DP-V1 services.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?