DOCA0256EN-01

Protection Trip Status

The table lists the protection trip status data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

Byte.Bit

RW

Type

Svd

Parameter name

1 33

40

1

40.0

R

BOOL

N

Thermal overload trip

40.1

R

BOOL

N

Locked rotor trip

40.2

R

BOOL

N

Stalled rotor trip

40.3

R

BOOL

N

Definite time overcurrent trip

40.4

R

BOOL

N

Normal inverse overcurrent trip

40.5

R

BOOL

N

Short time overcurrent trip

40.6

R

BOOL

N

Calculated ground current trip

40.7

R

BOOL

N

Measured ground current trip

1 33 41 1

41.0

R

BOOL

N

Phase under current trip

41.1

R

BOOL

N

Current imbalance trip

41.2

R

BOOL

N

Current phase loss trip

41.3

R

BOOL

N

Current phase reversal trip

41.4

R

BOOL

N

Phase under voltage trip

41.5

R

BOOL

N

Phase over voltage trip

41.6

R

BOOL

N

Voltage phase loss trip

41.7

R

BOOL

N

Voltage imbalance trip

1 33 42 1

42.0

R

BOOL

N

Voltage phase reversal trip

42.1

R

BOOL

N

Under frequency trip

42.2

R

BOOL

N

Over frequency trip

42.3

R

BOOL

N

Excessive start time trip

42.4

R

BOOL

N

Communication loss trip

42.5

R

BOOL

N

Over temperature trip

42.6

R

BOOL

N

Under power trip

42.7

R

BOOL

N

Over power trip

1 33 43 1

43.0

R

BOOL

N

Under power factor trip

43.1

Reserved

43.2

R

BOOL

N

Device Internal trip

Updated @D4

43.3

R

BOOL

N

HMI communication loss trip

Updated @D4

43.4–43.7

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?