Interlock Protection Pickup Status
The table lists the interlock protection pickup status data for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
Byte.Bit |
RW |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|
| 1 | 33 |
46 |
1 |
46.0 |
R |
BOOL |
N |
Interlock 1 pickup |
|
46.1 |
R |
BOOL |
N |
Interlock 2 pickup |
||||
|
46.2 |
R |
BOOL |
N |
Interlock 3 pickup |
||||
|
46.3 |
R |
BOOL |
N |
Interlock 4 pickup |
||||
|
46.4 |
R |
BOOL |
N |
Interlock 5 pickup |
||||
|
46.5 |
R |
BOOL |
N |
Interlock 6 pickup |
||||
|
46.6 |
R |
BOOL |
N |
Interlock 7 pickup |
||||
|
46.7 |
R |
BOOL |
N |
Interlock 8 pickup |
||||
| 1 | 33 | 47 | 1 |
47.0 |
R |
BOOL |
N |
Interlock 9 pickup |
|
47.1 |
R |
BOOL |
N |
Interlock 10 pickup |
||||
|
47.2 |
R |
BOOL |
N |
Interlock 11 pickup |
||||
|
47.3 |
R |
BOOL |
N |
Interlock 12 pickup |
||||
|
47.4–47.7 |
– |
– |
– |
Reserved |