DOCA0256EN-01

Wiring Diagram of LTMT Main Units Connected with Terminal Connector

LTMT Main Units Connected with Terminal Connector

The wiring diagram for connection of LTMT main units installed in an enclosure with the RS 485 bus via 4-terminal connectors is as follows:

Wiring Diagram of the Terminal Connector

Terminal Connector Assignment

Terminal

Signal

Description

A

RD-/TD- Negative data transmission

B

RD+/TD+ Positive data transmission

Blank

Not used

Shielded earth

Wiring Characteristics

The PROFIBUS DP cable must be a shielded twisted pair cable. PROFIBUS DP TSXPBSCA-00 shielded cable is recommended.

The following table describes the characteristics of screw terminals:

Pitch

5 mm

0.2 in.

Tightening torque

0.2 N•m

3 lb-in

Flat screwdriver

3 mm

0.10 in.

Screw terminals have an insulation rating of 320 Vac.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?