Under Frequency Protection
The table lists the under frequency protection data for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 6 |
64 |
2 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
| 1 | 6 |
66 |
2 |
RW |
1 |
%F* |
UINT16 |
90–100 |
94 |
Y |
Pickup |
| 1 | 6 |
68 |
2 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
| 1 | 6 |
70 |
2 |
RW |
1 |
%F* |
UINT16 |
90–100 |
94 |
Y |
Alarm level |
| 1 | 6 |
72 |
2 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
| 1 | 6 |
74 |
2 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
| 1 | 6 |
76 |
2 |
– |
– |
– |
– |
– |
– |
– |
Reserved |