Starter Settings
The table lists the starter settings for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 9 |
90 |
2 |
RW |
1 |
– |
UINT16 |
0: Motor 1: Heater |
0 |
Y |
Load type |
| 1 | 9 |
92 |
2 |
RW |
1 |
– |
UINT16 |
0–511 (step 1) |
1 |
Y |
Starter type |
| 1 | 9 |
94 |
2 |
RW |
1 |
– |
UINT16 |
0: Disable 1: HMI 2: DI 3: Communication |
0 |
Y |
Mode selection |
| 1 | 9 |
96 |
2 |
RW |
1 |
– |
BITMAP |
Bit 0: Disable Bit 1: HMI Bit 2: DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Local 1 start source |
| 1 | 9 |
98 |
2 |
RW |
1 |
– |
BITMAP |
Bit 0: Disable Bit 1: HMI Bit 2: DI Bit 3: Communication Bit 4: Custom logic |
0 |
Y |
Local 2 start source |
| 1 | 9 |
100 |
2 |
RW |
1 |
– |
BITMAP |
Bit 0: Disable Bit 1: HMI Bit 2: DI Bit 3: Communication Bit 4: Custom logic |
0 |
Y |
Local 3 start source |
| 1 | 9 |
102 |
2 |
RW |
1 |
– |
BITMAP |
Bit 0: Disable Bit 1: HMI Bit 2: DI Bit 3: Communication Bit 4: Custom logic |
0 |
Y |
Remote start source |
| 1 | 9 |
104 |
2 |
RW |
1 |
– |
BITMAP |
Bit 0: Disable Bit 1: HMI Bit 2: DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Local 1 stop source |
| 1 | 9 |
106 |
2 |
RW |
1 |
– |
BITMAP |
Bit 0: Disable Bit 1: HMI Bit 2: DI Bit 3: Communication Bit 4: Custom logic |
0 |
N |
Local 2 stop source |
| 1 | 9 |
108 |
2 |
RW |
1 |
– |
BITMAP |
Bit 0: Disable Bit 1: HMI Bit 2: DI Bit 3: Communication Bit 4: Custom logic |
0 |
Y |
Local 3 stop source |
| 1 | 9 |
110 |
2 |
RW |
1 |
– |
BITMAP |
Bit 0: Disable Bit 1: HMI Bit 2: DI Bit 3: Communication Bit 4: Custom logic |
0 |
N |
Remote stop source |
| 1 | 9 |
112 |
2 |
RW |
1 |
– |
UINT16 |
0: Momentary 1: Maintained |
0 |
Y |
Local DI start input |
| 1 | 9 |
114 |
2 |
RW |
1 |
– |
UINT16 |
0: Momentary 1: Maintained |
0 |
Y |
Remote DI start input |
| 1 | 9 |
116 |
2 |
RW |
1 |
– |
UINT16 |
0: Momentary 1: Maintained |
0 |
Y |
Custom start input |
| 1 | 9 |
118 |
2 |
RW |
1 |
– |
UINT16 |
0: Bump 1: Bumpless |
0 |
Y |
Mode transfer |
| 1 | 9 |
120 |
2 |
RW |
1 |
– |
UINT16 |
0: Momentary 1: Maintained |
0 |
Y |
Communication start input |
| 1 | 9 |
122 |
4 |
RW |
– | – |
UINT16 |
– | – | – | Reserved |
| 1 | 9 |
126 |
2 |
RW |
1 |
– | –
UINT16 |
0: Disable 1: Enable |
0 |
N |
Change direction |
| 1 | 9 |
128 |
2 |
RW |
0.01 |
s |
UINT16 |
1–60000 (step 1) |
50 |
Y |
Feedback response time |
| 1 | 9 |
130 |
2 |
RW |
0.01 |
s |
UINT16 |
1–60000 (step 1) |
50 |
Y |
Motor current sensing time |
| 1 | 9 |
132 |
2 |
RW |
0.01 |
s |
UINT16 |
1–60000 (step 1) |
6000 |
Y |
Interlocking time |
| 1 | 9 |
134 |
2 |
RW |
0.01 |
s |
UINT16 |
1–60000 (step 1) |
1000 |
Y |
Time in star |
| 1 | 9 |
136 |
2 |
RW |
0.01 |
s |
UINT16 |
1–60000 (step 1) |
30 |
Y |
Changeover time |
| 1 | 9 |
138 |
2 |
RW |
0.01 |
s |
UINT16 |
1–60000 (step 1) |
1 |
Y |
Main contactor turn off time |
| 1 | 9 |
140 |
2 |
RW |
0.01 | s |
UINT16 |
1–60000 (step 1) |
1 |
Y |
Capacitor control time |
| 1 | 9 |
142 |
6 |
RW |
– | – | – | – | – | – |
Reserved |
| 1 | 9 |
148 |
2 |
RW |
1 |
– |
UINT16 |
0: Three phase 1: Single phase |
0 |
Y | Number of phases |
| 1 | 9 |
150 |
2 |
RW |
1 |
– |
UINT16 |
0: DI+Current based 1: Current based |
1 |
Y |
Stop detection |
| 1 | 9 | 152 | 2 | RW | 1 | – |
UINT16 |
0: Disable 1: Enable |
0 |
Y |
Forced start function |