DOCA0256EN-01

Module in GSD File

Overview

The TeSys Tera system is presented as a modular device on the PROFIBUS DP network. A General Station Description (GSD) file describes the TeSys Tera system. The GSD file can be used by any PROFIBUS DP configuration tool to get information about the device.

GSD File

The file for the PROFIBUS DP LTMT main unit is called CCCCCC.GSD.

  • For the GSD files 2.01, CCCCCC stands for TT2011AE_0102.gsd.

The GSD files and icons associated with the LTMT main unit can be downloaded from www.se.com/ww/en/download/.

WARNING
UNINTENDED BEHAVIOUR OF EQUIPMENT
  • Do not modify the GSD file in any manner.
  • Modifying the GSD file can cause unpredictable behavior of the devices.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: If the GSD file is modified in any manner, the Schneider Electric guarantee is immediately void.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?