DOCA0256EN-01

Thermal Overload Protection

The table lists the thermal overload protection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 5

0

2

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm and Trip

3

Y

Function setting

1 5

2

2

RW

0.01

UINT16

100–150
(step 5)

115

Y

Service factor

1 5

4

2

RW

1

UINT16

5–40
(step 5)

10

Y

Trip class

1 5

6

2

RW

1

%TM*

UINT16

80–100
(step 5)

80

Y

Alarm level

1 5

8

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

8

Y

Reset mode*

1 5

10

2

RW

1

%TM*

UINT16

30–95
(step 5)

90

Y

Thermal reset level

1 5

12

2

RW

1

%TM*

UINT16

5–100
(step 5)

90

Y

Start inhibit level

1 5

14

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Cool down function

1 5

16

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Cool down time

1 5

18

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Pause function

1 5

20

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Pause time

1 5

22

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Block function

1 5

24

2

RW

1

%TM*

UINT16

80–95
(step 5)

80

Y

Block level

1 5

26

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Block time

1 5 28 2 RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Auxiliary fan

1 5 30

6

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?