DOCA0256EN-01

Digital Inputs Settings

The table lists the digital inputs settings for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 27

0

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 1 trigger type

1 27

2

2

RW

1

UINT16

0–38
(step 1)

4

Y

Digital input 1 input source

1 27

4

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 1 validation time

1 27

6

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

1

Y

Digital input 2 trigger type

1 27

8

2

RW

1

UINT16

0–38
(step 1)

6

Y

Digital input 2 input source

1 27

10

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 2 validation time

1 27

12

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 3 trigger type

1 27

14

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 3 input source

1 27

16

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 3 validation time

1 27

18

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 4 trigger type

1 27

20

2

RW

1

UINT16

0–38
(step 1)

30

Y

Digital input 4 input source

1 27

22

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 4 validation time

1 27

24

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 5 trigger type

1 27

26

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 5 input source

1 27

28

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 5 validation time

1 27

30

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 6 trigger type

1 27

32

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 6 input source

1 27

34

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 6 validation time

1 27

36

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 7 trigger type

1 27

38

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 7 input source

1 27

40

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 7 validation time

1 27

42

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 8 trigger type

1 27

44

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 8 input source

1 27

46

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 8 validation time

1 27

48

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 9 trigger type

1 27

50

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 9 input source

1 27

52

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 9 validation time

1 27

54

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 10 trigger type

1 27

56

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 10 input source

1 27

58

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 10 validation time

1 27

60

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 11 trigger type

1 27

62

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 11 input source

1 27

64

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 11 validation time

1 27

66

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 12 trigger type

1 27

68

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 12 input source

1 27

70

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 12 validation time

1 27

72

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 13 trigger type

1 27

74

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 13 input source

1 27

76

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 13 validation time

1 27

78

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 14 trigger type

1 27

80

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 14 input source

1 27

82

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 14 validation time

1 27

84

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 15 trigger type

1 27

86

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 15 input source

1 27

88

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 15 validation time

1 27

90

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 16 trigger type

1 27

92

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 16 input source

1 27

94

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 16 validation time

1 27

96

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 17 trigger type

1 27

98

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 17 input source

1 27

100

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 17 validation time

1 27

102

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 18 trigger type

1 27

104

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 18 input source

1 27

106

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 18 validation time

1 27

108

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 19 trigger type

1 27

110

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 19 input source

1 27

112

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 19 validation time

1 27

114

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 20 trigger type

1 27

116

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 20 input source

1 27

118

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 20 validation time

1 27

120

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 21 trigger type

1 27

122

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 21 input source

1 27

124

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 21 validation time

1 27

126

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 22 trigger type

1 27

128

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 22 input source

1 27

130

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 22 validation time

1 27

132

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 23 trigger type

1 27

134

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 23 input source

1 27

136

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 23 validation time

1 27

138

2

RW

1

UINT16

  • 0: Active high

  • 1: Active low

0

Y

Digital input 24 trigger type

1 27

140

2

RW

1

UINT16

0–38
(step 1)

0

Y

Digital input 24 input source

1 27

142

2

RW

1

ms

UINT16

0–60000
(step 1)

10

Y

Digital input 24 validation time

1 27

144–190

2

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?