Permissive Command Status
The table lists the permissive command status data for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
Byte.Bit |
RW |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|
| 1 | 33 |
68 |
1 |
68.0 |
R |
BOOL |
N |
Status - Permissive command 1 |
|
68.1 |
R |
BOOL |
N |
Status - Permissive command 2 |
||||
|
68.2 |
R |
BOOL |
N |
Status - Permissive command 3 |
||||
|
68.3 |
R |
BOOL |
N |
Status - Permissive command 4 |
||||
|
68.4 |
R |
BOOL |
N |
Status - Permissive command 5 |
||||
|
68.5 |
R |
BOOL |
N |
Status - Permissive command 6 |
||||
|
68.6 |
R |
BOOL |
N |
Status - Permissive command 7 |
||||
|
68.7 |
R |
BOOL |
N |
Status - Permissive command 8 |
||||
| 1 | 33 | 69 | 1 | 69.0–69.7 |
– |
– |
– |
Reserved |
| 1 | 33 | 70 | 1 | 70.0–70.7 | – | – | – | Reserved |
| 1 | 33 | 71 | 1 | 71.0–71.7 | – | – | – | Reserved |