DOCA0256EN-01

Under Power Factor Protection

The table lists the under power factor protection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 6

120

2

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

1 6

122

2

RW

0.10

PF

UINT16

40–100
(step 1)

60

Y

Pickup

1 6

124

2

RW

0.1

s

UINT16

1–60000
(step 1)

1

Y

Time delay

1 6

126

2

RW

0.10

PF

UINT16

40–100
(step 1)

60

Y

Alarm level

1 6

128

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

1 6

130

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

1 6

132

2

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?