DOCA0256EN-01

Short Time Overcurrent Protection

The table lists the short time overcurrent protection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 5

90

2

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

1 5

92

2

RW

1

%IFLC*

UINT16

100–1000
(step 1)

100

Y

Pickup

1 5

94

2

RW

0.01

s

UINT16

5–1000
(step 1)

5

Y

Time delay

1 5

96

2

RW

1

%IFLC*

UINT16

100–1000
(step 1)

100

Y

Alarm level

1 5

98

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

1 5

100

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

1 5

102

2

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?