Phase Under Current Protection
The table lists the phase under current protection data for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 5 |
132 |
2 |
RW |
1 |
– |
UINT16 |
|
1 |
Y |
Function setting |
| 1 | 5 |
134 |
2 |
RW |
1 |
%IFLC* |
UINT16 |
15–100 |
50 |
Y |
Pickup |
| 1 | 5 |
136 |
2 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
100 |
Y |
Time delay |
| 1 | 5 |
138 |
2 |
RW |
1 |
%IFLC* |
UINT16 |
15–100 |
50 |
Y |
Alarm level |
| 1 | 5 |
140 |
2 |
RW |
1 |
– |
BITMAP |
|
8 |
Y |
Reset mode |
| 1 | 5 |
142 |
2 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
50 |
Y |
Auto-Reset delay |
| 1 | 5 |
144 |
4 |
– |
– |
– |
– |
– |
– |
– |
Reserved |