Device Internal Status (LTMTCT/LTMTCTV Sensor Module)
The table lists the device internal error detection setting (LTMTCT/LTMTCTV sensor module) data for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
Byte.Bit |
RW |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|
| 1 | 33 |
80 |
1 |
80.0 |
R |
BOOL |
N |
Watchdog timeout detected |
|
80.1 |
R |
BOOL |
N |
ADC conversion error detected |
||||
|
80.2 |
R |
BOOL |
N |
Flash error detected |
||||
|
80.3 |
– |
– |
– |
Reserved |
||||
|
80.4 |
R |
BOOL |
N |
Voltage configuration not detected |
||||
|
80.5 |
– |
– |
– |
Reserved |
||||
|
80.6 |
R |
BOOL |
N |
Calibration error detected |
||||
|
80.7 |
R |
BOOL |
N |
VL1 measurement error detected |
||||
| 1 | 33 | 81 | 1 |
81.0 |
R |
BOOL |
N |
VL2 measurement error detected |
|
81.1 |
R |
BOOL |
N |
VL3 measurement error detected |
||||
|
81.2 |
R |
BOOL |
N |
IL1 low gain measurement error detected |
||||
|
81.3 |
R |
BOOL |
N |
IL1 high gain measurement error detected |
||||
|
81.4 |
R |
BOOL |
N |
IL2 low gain measurement error detected |
||||
|
81.5 |
R |
BOOL |
N |
IL2 high gain measurement error detected |
||||
|
81.6 |
R |
BOOL |
N |
IL3 low gain measurement error detected |
||||
|
81.7 |
R |
BOOL |
N |
IL3 high gain measurement error detected |
||||
| 1 | 33 | 82 | 1 |
82.0–82.7 |
– |
– |
– |
Reserved |
| 1 | 33 | 83 | 1 |
83.0–83.7 |
– |
– |
– |
Reserved |