DOCA0256EN-01

Identification and Monitoring Data

Overview

The call mechanism in use for the Identification and Monitoring (I&M) functions are defined within the standard IEC 61158-6, chapter 6.1. The data structure of a call mechanism consists of DP-V1 header, call header, and the body.

Request

Definition

Number of Bytes

Value

Comment

Category

FUNCTION_NUM

1 octet

5 Fh

Indicates write fix

DP-V1 header

Slot number

1 octet

0 to 255

Variable

Index

1 octet

255

Fix

Length of net data

1 octet

68 (with body)

Length of I&M data set

EX-TENDED_FUNCTION_NUM

1 octet

08 h

Indicates CALL fix

Call header

Reserved

1 octet

0 h

Fix

IM_INDEX

2 octets

65000 to 65199

Reserved for I&M

IM_FUNCTION

64 octets

In accordance with the definition

I&M3 descriptor

Body

NOTE: In case of Read Log, there is no item within the write call.

Response

Definition

Number of Bytes

Value

Comment

Category

FUNCTION_NUM

1 octet

5 Eh

Indicates read fix

DP-V1 header

Slot number

1 octet

0 to 255

Variable

Index

1 octet

255

Fix

Length of net data

1 octet

68 (with body)

Length of I&M data set

EX-TENDED_FUNCTION_NUM

1 octet

08 h

Indicates CALL fix

Call header

Reserved

1 octet

0 h

Fix

IM_INDEX

2 octets

65000 to 65199

Reserved for I&M

IM_FUNCTION

64 octets

In accordance with the definition

I&M3 descriptor

Body

NOTE: In case of Write Log, there is no item within the read call.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?