Maximum Number of Starts
The table lists the maximum number of starts data for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 7 |
32 |
2 |
RW |
1 |
– |
UINT16 |
|
1 |
Y |
Function setting |
| 1 | 7 |
34 |
2 |
RW |
1 |
– |
UINT16 |
1–30 |
6 |
Y |
Permissive starts |
| 1 | 7 |
36 |
2 |
RW |
1 |
min |
UINT16 |
15–60 |
30 |
Y |
Reference time |
| 1 | 7 |
38 |
2 |
RW |
1 |
min |
UINT16 |
1–120 |
5 |
Y |
Inhibit period |
| 1 | 7 |
40 |
2 |
RW |
1 |
min |
UINT16 |
0–120 |
0 |
Y |
Time between starts |
| 1 | 7 |
42 |
6 |
– |
– |
– |
– |
– |
– |
– |
Reserved |