DOCA0256EN-01

Motor Stop Error Detection

The table lists the motor stop error detection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 7

48

2

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

Y

Function setting

1 7

50

2

RW

0.1

s

UINT16

1–60000
(step 1)

10

Y

Time delay

1 7

52

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

1 7

54

4

RW

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?