Hysteresis Settings
The table lists the hysteresis settings for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 29 |
0 |
2 |
RW |
1 |
% |
UINT16 |
3–15 (step 1) |
3 |
Y |
Current protection |
| 1 | 29 |
2 |
2 |
RW |
1 |
% |
UINT16 |
3–15 (step 1) |
3 |
Y |
Voltage protection |
| 1 | 29 |
4 |
2 |
RW |
1 |
% |
UINT16 |
1–15 (step 1) |
3 |
Y |
Frequency protection |
| 1 | 29 |
6 |
2 |
RW |
1 |
% |
UINT16 |
3–15 (step 1) |
3 |
Y |
Power protection |
| 1 | 29 |
8 |
2 |
RW |
1 |
mA |
UINT16 |
1–3 (step 1) |
1 |
Y |
Analog input protection |
| 1 | 29 |
8–10 |
2 |
– |
– |
– |
– |
– |
– |
– |
Reserved |