Device Internal Status
The table lists the device internal status for the PROFIBUS DP communication.
| Slot | Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|---|---|
| 1 | 7 |
58 |
2 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
10 |
Y |
Time delay |
| 1 | 7 |
59 |
2 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
| 1 | 7 |
60 |
2 |
RW |
– |
– |
UINT16 |
|
1 | N |
Internal temperature alarm |
| 1 | 7 |
61 |
2 |
– |
– |
– |
– |
– |
– |
– |
Reserved |