DOCA0256EN-01

Protection Alarm Status

The table lists the protection alarm status data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

Byte.Bit

RW

Type

Svd

Parameter name

1 33

32

1

32.0

R

BOOL

N

Thermal overload alarm

32.1

R

BOOL

N

Locked rotor alarm

32.2

R

BOOL

N

Stalled rotor alarm

32.3

R

BOOL

N

Definite time overcurrent alarm

32.4

R

BOOL

N

Normal inverse overcurrent alarm

32.5

R

BOOL

N

Short time overcurrent alarm

32.6

R

BOOL

N

Calculated ground current alarm

32.7

R

BOOL

N

Measured ground current alarm

1 33 33 1

33.0

R

BOOL

N

Phase under current alarm

33.1

R

BOOL

N

Current imbalance alarm

33.2

R

BOOL

N

Current phase loss alarm

33.3

R

BOOL

N

Current phase reversal alarm

33.4

R

BOOL

N

Phase under voltage alarm

33.5

R

BOOL

N

Phase over voltage alarm

33.6

R

BOOL

N

Voltage phase loss alarm

33.7

R

BOOL

N

Voltage imbalance alarm

1 33 34 1

34.0

R

BOOL

N

Voltage phase reversal alarm

34.1

R

BOOL

N

Under frequency alarm

34.2

R

BOOL

N

Over frequency alarm

34.3

Reserved

34.4

R

BOOL

N

Communication loss alarm

34.5

R

BOOL

N

Over temperature alarm

34.6

R

BOOL

N

Under power alarm

34.7

R

BOOL

N

Over power alarm

1 33 35 1

35.0

R

BOOL

N

Under power factor alarm

35.1

Reserved

35.2

R

BOOL

N

Device internal temperature alarm

35.3

R

BOOL

N

HMI communication loss alarm

35.4–35.7

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?