DOCA0256EN-01

Digital Input Interlock Protection Settings

Description

The order and the description of the settings for digital input 1 are valid for the other digital inputs.

Slot Index

Byte offset

Size (in bytes)

RW

Description

1 8

0

10

RW

Digital input 1 interlock protection settings

1 8

10

10

RW

Digital input 2 interlock protection settings

1 8

20

10

RW

Digital input 3 interlock protection settings

1 8

30

10

RW

Digital input 4 interlock protection settings

1 8

40

10

RW

Digital input 5 interlock protection settings

1 8

50

10

RW

Digital input 6 interlock protection settings

1 8

60

10

RW

Digital input 7 interlock protection settings

1 8

70

10

RW

Digital input 8 interlock protection settings

1 8

80

10

RW

Digital input 9 interlock protection settings

1 8

90

10

RW

Digital input 10 interlock protection settings

1 8

100

10

RW

Digital input 11 interlock protection settings

1 8

110

10

RW

Digital input 12 interlock protection settings

Digital Input 1 Interlock Protection Settings

The table lists the digital input 1 interlock protection settings for the PROFIBUS DP communication.

Slot Index

Byte offset

Size
(in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 8

0

2

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

1 8

2

2

RW

0.1

s

UINT16

0–6000
(step 1)

0

Y

Time delay

1 8

4

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

1 8

6

2

RW

0.1

s

UINT16

0–6000
(step 1)

0

Y

Auto-Reset delay

1 8

8

2

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?