DOCA0256EN-01

Detected Internal Error Logs

Description

The last 20 detected internal errors are recorded by the LTMT main unit.

Each detected internal error log is composed of 16 bytes. The data of each detected internal error log are organized as the data of Detected Internal Error Log 1 Data.

Slot Index Byte offset Size (in bytes) Detected internal error log
1 25

0

16 Detected internal error log 1

16

16

Detected internal error log 2

32

16

Detected internal error log 3

48

16

Detected internal error log 4

64

16

Detected internal error log 5

80

16

Detected internal error log 6

96

16

Detected internal error log 7

112

16

Detected internal error log 8

128

16

Detected internal error log 9

144

16

Detected internal error log 10

160

16

Detected internal error log 11

176

16

Detected internal error log 12

192

16

Detected internal error log 13

208

16

Detected internal error log 14

224

16

Detected internal error log 15

1 26

0

16

Detected internal error log 16

16

16

Detected internal error log 17

32

16

Detected internal error log 18

48

16

Detected internal error log 19

64

16

Detected internal error log 20

Detected Internal Error Log 1 Data

Slot

Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Svd

Parameter name

1 25 0 8 R

UINT16

Y

Date and Time

1 25 8 2 R

UINT16

Y

Detected Internal Error Code

1 25 10 6 R

Y Reserved
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?