DOCA0256EN-01

Voltage Imbalance Protection

The table lists the voltage imbalance protection data for the PROFIBUS DP communication.

Slot Index

Byte offset

Size (in bytes)

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

1 6

40

2

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

3

Y

Function setting

1 6

42

2

RW

1

%Vn

UINT16

5–50
(step 5)

10

Y

Pickup

1 6

44

2

RW

0.1

s

UINT16

1–60000
(step 1)

100

Y

Time delay

1 6

46

2

RW

1

%Vn

UINT16

5–50
(step 5)

10

Y

Alarm level

1 6

48

2

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI

  • Bit 2: Communication

  • Bit 3: Auto

3

Y

Reset mode

1 6

50

2

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

1 6

52

2

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?