Event Logs
Description
The last 100 events are recorded by the LTMT main unit.
Each event log is composed of 16 bytes. The data of each trip log are organized as the data of Event Log 1 Data.
| Slot | Index | Byte offset | Size (in bytes) | Event log |
|---|---|---|---|---|
| 1 | 18 |
0 |
16 | Event log 1 |
|
16 |
16 |
Event log 2 |
||
|
32 |
16 |
Event log 3 |
||
|
48 |
16 |
Event log 4 |
||
|
64 |
16 |
Event log 5 |
||
|
80 |
16 |
Event log 6 |
||
|
96 |
16 |
Event log 7 |
||
|
112 |
16 |
Event log 8 |
||
|
128 |
16 |
Event log 9 |
||
|
144 |
16 |
Event log 10 |
||
|
160 |
16 |
Event log 11 |
||
|
176 |
16 |
Event log 12 |
||
|
192 |
16 |
Event log 13 |
||
|
208 |
16 |
Event log 14 |
||
|
224 |
16 |
Event log 15 |
||
| 1 | 19 |
0 |
16 |
Event log 16 |
|
16 |
16 |
Event log 17 |
||
|
32 |
16 |
Event log 18 |
||
|
48 |
16 |
Event log 19 |
||
|
64 |
16 |
Event log 20 |
||
|
80 |
16 |
Event log 21 |
||
|
96 |
16 |
Event log 22 |
||
|
112 |
16 |
Event log 23 |
||
|
128 |
16 |
Event log 24 |
||
|
144 |
16 |
Event log 25 |
||
|
160 |
16 |
Event log 26 |
||
|
176 |
16 |
Event log 27 |
||
|
192 |
16 |
Event log 28 |
||
|
208 |
16 |
Event log 29 |
||
|
224 |
16 |
Event log 30 |
||
| 1 | 20 |
0 |
16 |
Event log 31 |
|
16 |
16 |
Event log 32 |
||
|
32 |
16 |
Event log 33 |
||
|
48 |
16 |
Event log 34 |
||
|
64 |
16 |
Event log 35 |
||
|
80 |
16 |
Event log 36 |
||
|
96 |
16 |
Event log 37 |
||
|
112 |
16 |
Event log 38 |
||
|
128 |
16 |
Event log 39 |
||
|
144 |
16 |
Event log 40 |
||
|
160 |
16 |
Event log 41 |
||
|
176 |
16 |
Event log 42 |
||
|
192 |
16 |
Event log 43 |
||
|
208 |
16 |
Event log 44 |
||
|
224 |
16 |
Event log 45 |
||
| 1 | 21 |
0 |
16 |
Event log 46 |
|
16 |
16 |
Event log 47 |
||
|
32 |
16 |
Event log 48 |
||
|
48 |
16 |
Event log 49 |
||
|
64 |
16 |
Event log 50 |
||
|
80 |
16 |
Event log 51 |
||
|
96 |
16 |
Event log 52 |
||
|
112 |
16 |
Event log 53 |
||
|
128 |
16 |
Event log 54 |
||
|
144 |
16 |
Event log 55 |
||
|
160 |
16 |
Event log 56 |
||
|
176 |
16 |
Event log 57 |
||
|
192 |
16 |
Event log 58 |
||
|
208 |
16 |
Event log 59 |
||
|
224 |
16 |
Event log 60 |
||
| 1 | 22 |
0 |
16 |
Event log 61 |
|
16 |
16 |
Event log 62 |
||
|
32 |
16 |
Event log 63 |
||
|
48 |
16 |
Event log 64 |
||
|
64 |
16 |
Event log 65 |
||
|
80 |
16 |
Event log 66 |
||
|
96 |
16 |
Event log 67 |
||
|
112 |
16 |
Event log 68 |
||
|
128 |
16 |
Event log 69 |
||
|
144 |
16 |
Event log 70 |
||
|
160 |
16 |
Event log 71 |
||
|
176 |
16 |
Event log 72 |
||
|
192 |
16 |
Event log 73 |
||
|
208 |
16 |
Event log 74 |
||
|
224 |
16 |
Event log 75 |
||
| 1 | 23 |
0 |
16 |
Event log 76 |
|
16 |
16 |
Event log 77 |
||
|
32 |
16 |
Event log 78 |
||
|
48 |
16 |
Event log 79 |
||
|
64 |
16 |
Event log 80 |
||
|
80 |
16 |
Event log 81 |
||
|
96 |
16 |
Event log 82 |
||
|
112 |
16 |
Event log 83 |
||
|
128 |
16 |
Event log 84 |
||
|
144 |
16 |
Event log 85 |
||
|
160 |
16 |
Event log 86 |
||
|
176 |
16 |
Event log 87 |
||
|
192 |
16 |
Event log 88 |
||
|
208 |
16 |
Event log 89 |
||
|
224 |
16 |
Event log 90 |
||
| 1 | 24 |
0 |
16 |
Event log 91 |
|
16 |
16 |
Event log 92 |
||
|
32 |
16 |
Event log 93 |
||
|
48 |
16 |
Event log 94 |
||
|
64 |
16 |
Event log 95 |
||
|
80 |
16 |
Event log 96 |
||
|
96 |
16 |
Event log 97 |
||
|
112 |
16 |
Event log 98 |
||
|
128 |
16 |
Event log 99 |
||
|
144 |
16 |
Event log 100 |
Event Log 1 Data
|
Slot |
Index |
Byte offset |
Size (in bytes) |
RW |
X |
Unit |
Type |
Svd |
Parameter name |
|---|---|---|---|---|---|---|---|---|---|
| 1 | 18 | 0 | 8 | R |
– |
– |
UINT16 |
Y | |
| 1 | 18 | 8 | 2 | R |
– |
– |
UINT16 |
Y | |
| 1 | 18 | 10 | 6 | R |
– |
– |
– |
Y | Reserved |