DOCA0256EN-01

Data Mapping

For acyclic DP-V1 access, a mechanism based on slot or index and length addressing is implemented in the LTMT main unit.

Slot

Index

Read/Write

Description

1

0

Read

Diagnostic Data

1

1

Read

Input Data

1

2

Read/Write

Output Data

1

3

Read

Measurement and Monitoring Data

1

4

Read

Statistic Data

1

5

Read/Write

Current Protection Settings

1

6

Read/Write

Voltage Protection Settings

1

7

Read/Write

Motor Control Function Settings

1

8

Read/Write

Digital Input Interlock Protection Settings

1

9

Read/Write

General Settings

1

10

Read/Write

Communication Parameters

1

11–17

Read

Trip Logs

1

18–24

Read

Event Logs

1

25–26

Read

Detected Internal Error Logs

1

27

Read

Digital Inputs Settings

1

28

Read/Write

Digital Output Settings

1

29

Read/Write

Hysteresis Settings

1

30–32

Read/Write

Motor Start Logs

1

33

Read

Status Data

1

34

Read

Reserved

1

35

Read

Reserved

1

36

Read/Write

Reserved

Table Format

The PROFIBUS DP data tables have the following columns:

Slot Index

Byte offset

Size (in bytes)

Byte.Bit

RW

X

Unit

Type

Range

Default value

Svd

Parameter name

Designation

Description

Slot/Index DP-V1 addressing mechanism

Byte offset

Number of bytes from the index.

Size (in bytes)

Number of bytes that need to be read or written to access the complete information.

Byte.Bit

Number of the bit in a byte, for boolean data only.

RW

Whether the data is read only (R) or read-write (RW).

X

Scale factor:

  • A scale of 1 means that the value of the data is the right one with the unit indicated.

  • A scale of 10 means that the data contains the value multiplied by 10. The actual value is therefore the value of the data divided by 10.

  • A scale of 0.1 means that the data contains the value multiplied by 0.1. The actual value is therefore the value of the data multiplied by 10.

Unit

Unit of the value, only for integer data types.

Type

Coding data type (see Data Types table below).

Range

Range of permitted values for the variable, usually a subset of what the format allows. Only for integer data types that can be written. For BITMAP data type, the content range does not exist.

Default Value

Default value for the parameter.

Svd

Value saved when the power supply to the TeSys Tera system is switched off:

  • Y: the value of the data is saved.

  • N: the value is lost.

NOTE: The saved values are retrieved when the power supply to the TeSys Tera system is switched on.

Parameter name

Information about the data and the restrictions that apply.

Data Types

Name

Description

Range

INT16

16-bit signed integer (1 word)

-32768...+32767

UINT16

16-bit unsigned integer (1 word)

0...65535

UINT32

32-bit unsigned integer (2 words)

0...4 294 967 295

UINT64

64-bit unsigned integer (4 words)

0...18 446 744 073 709 600 000

BOOL

1-bit data

0–1

BITMAP

16-bit field (1 word)

UINT8

8-bit unsigned character

0–255

Example of Endianness

Data Type Value Value in Hexadecimal Big-endian Little-endian
UINT16/INT16 1000 03E8 03 E8 E8 03
UINT32/INT32 70000 00011170 00 01 11 70 70 11 01 00
UINT64/INT64 100000 00000000000186A0 00 00 00 00 00 01 86 A0 A0 86 01 00 00 00 00 00

Date and Time

The date and time of events is coded in 8 bytes.

Byte offset Size (in bytes) Parameter name
0 1 Day (1–31)
1 1 Month (1–12)
2 1 Year (0–99)
3 1 Hour (0–23)
4 1 Minute (0–59)
5 1 Second (0–59)
6 2 Millisecond (0–999)

For setting date and time, refer to the Real-Time Clock Settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?